Skip to main content
Dallas-Fort Worth Fall 2020
High-Performance Power Conversion Seminar & Workshops View Agenda Register now

Keynote speaker:
Dr. Ray Ridley

President, Ridley Engineering, Inc.

Dr. Ridley has been designing, researching, and teaching power electronics for over 40 years. His teaching style is renowned for applying advanced theory to practical design. He is very active in creating software and hardware development tools for designers. Thousands of engineers in 72 countries have taken his courses and use his products in the design process. His landmark work on current-mode control defined how the system should be analyzed and has remained the standard for over 30 years. Learn more

Dr. Ray Ridley

日程

October 3, 2019

Mouser Corporate Headquarters 1000 N Main St, Mansfield, TX 76063


注册/技术展台开放


Welcome


Keynote by Dr. Ray Ridley


Coffee break


研讨会:EMI 挑战及故障排除技术

应用工程师主讲

如果没有适当的考虑,EMI 可能会阻挠项目进程,造成代价高昂的延迟。通过一个实际故障排除示例,您将了解基本的 EMI 测量、共模和差模噪声源及识别方法、传导 EMI 预合规性测试以及布局问题等。

研讨会:正确完成模块化 DC-DC 系统设计

应用工程师主讲

现实世界的系统不仅仅包括 DC-DC 转换器本身。通过一个案例来探讨模块集成至 DC-DC 系统的需求,您将学习到输入输出、滤波、保护、与电源的兼容性以及负载动态等主题。


Lunch


研讨会:避免常见的 AC-DC 设计缺陷

应用工程师主讲

AC-DC 前端模块的设计过程比较复杂。本课程将提供一个获得成功的简单方法,涵盖诸如电源阻抗注意事项、涌流、滤波器共振和阻尼、PFC、故障、保险装置、系统稳定性和安全性等主题。

研讨会:高性能 PCB 布局和散热设计技术

应用工程师主讲

我们的专家将分享他们的优化技术,解决以下问题:应用散热模型和仿真、支持高效率热管理的 PCB 布局、在高密度、大电流应用中的电源/信号路由和完整性,最大限度降低电路板损耗并最大限度提高性能。


Coffee break


研讨会:避免常见的 AC-DC 设计缺陷

应用工程师主讲

AC-DC 前端模块的设计过程比较复杂。本课程将提供一个获得成功的简单方法,涵盖诸如电源阻抗注意事项、涌流、滤波器共振和阻尼、PFC、故障、保险装置、系统稳定性和安全性等主题。

研讨会:正确完成模块化 DC-DC 系统设计

应用工程师主讲

现实世界的系统不仅仅包括 DC-DC 转换器本身。通过一个案例来探讨模块集成至 DC-DC 系统的需求,您将学习到输入输出、滤波、保护、与电源的兼容性以及负载动态等主题。


Wrap up & Networking


Our sponsor

Mouser

Registration

This event is a professional seminar with limited seats. Your company information is required for your registration.  Limit five (5) attendees from each company.

请输入一个有效的

Register

错误

提交表单时发生错误